The ADP210x_{...}.xls is a stand-alone tool for generating a power supply design that employs an appropriate integrated switch ADI regulator: ADP2102, ADP2105, ADP2106, and ADP2107.

IMPORTANT: You must enable macros when Microsoft Excel asks you as the file is being opened.

This Excel tool produces a schematic, bill of materials, and performance specifications including efficiency based on the user's preference for size, efficiency, and cost.

Note:  Microsoft Excel is dependent on the language setting Microsoft Windows for the indication of a decimal point. Minor issues may arise when this file is saved using US English notation and then read/run in Excel of another language.  Changing the decimal notation in the input entries (such as "2.7" to "2,7") should resolve this.

Analog Devices, Inc.
www.analog.com