Analog Devices Wi-Fi Software Reference Manual  Release 1.0.0
MQTTPublish.h
1 /*******************************************************************************
2  * Copyright (c) 2014 IBM Corp.
3  *
4  * All rights reserved. This program and the accompanying materials
5  * are made available under the terms of the Eclipse Public License v1.0
6  * and Eclipse Distribution License v1.0 which accompany this distribution.
7  *
8  * The Eclipse Public License is available at
9  * http://www.eclipse.org/legal/epl-v10.html
10  * and the Eclipse Distribution License is available at
11  * http://www.eclipse.org/org/documents/edl-v10.php.
12  *
13  * Contributors:
14  * Ian Craggs - initial API and implementation and/or initial documentation
15  * Xiang Rong - 442039 Add makefile to Embedded C client
16  *******************************************************************************/
17 
18 #ifndef MQTTPUBLISH_H_
19 #define MQTTPUBLISH_H_
20 
21 #if !defined(DLLImport)
22  #define DLLImport
23 #endif
24 #if !defined(DLLExport)
25  #define DLLExport
26 #endif
27 
28 DLLExport int MQTTSerialize_publish(unsigned char* buf, int buflen, unsigned char dup, int qos, unsigned char retained, unsigned short packetid,
29  MQTTString topicName, unsigned char* payload, int payloadlen);
30 
31 DLLExport int MQTTDeserialize_publish(unsigned char* dup, int* qos, unsigned char* retained, unsigned short* packetid, MQTTString* topicName,
32  unsigned char** payload, int* payloadlen, unsigned char* buf, int len);
33 
34 DLLExport int MQTTSerialize_puback(unsigned char* buf, int buflen, unsigned short packetid);
35 DLLExport int MQTTSerialize_pubrel(unsigned char* buf, int buflen, unsigned char dup, unsigned short packetid);
36 DLLExport int MQTTSerialize_pubcomp(unsigned char* buf, int buflen, unsigned short packetid);
37 
38 #endif /* MQTTPUBLISH_H_ */
Definition: MQTTPacket.h:81