Readme file for prog106x software ----------------------------------- prog106x is a command line executable, as such it has no GUI component. The tool is designed to allow users to detect/erase/download/upload/verify the EEPROM contents of ADM1062-ADM1069 devices. A User Guide describing how to use the software is installed in the Start menu, in the Analog Devices >> prog106x folder. IMPORTANT ********** The USB to I2C dongle used by this software requires device drivers to be installed prior to use. These drivers are installed as part of the standard ADM106x Evalation GUI software. This is available from the 'Evaluation Boards/Tools' section of the ADM1062-ADM1069 page at http://www.analog.com. The prog106x software will not work correctly without the drivers being installed first. Minimum system requirements **************************** Windows XP SP2 500 MHz Processor 80 Meg free disc space 256Mb RAM Minimum viewing resolution *************************** 800 x 600 High colour (16 bit) prog106x Software history ************************** 1.0.2, July 27th 2009 First public version 1.1.0, April 20th 2010 Chnaged driver to use NI VISA 2.0.0, April 10th 2012 Added support of SDP 2.0.1, May 17th 2012 Added command line arguments to support SE restart after download, batch processing and repeat download. Fixed a problem with detecting I2C interfaces, where if the USB-SDP-CABLEZ interface had never been connected to a PC, it could prevent other I2C interfaces from being detected.