# SPDX-License-Identifier: GPL-2.0-or-later OR GFDL-1.2-no-invariants-or-later

OpenOCD licensing rules
=======================

The OpenOCD source code is provided under the terms of the GNU General
Public License version 2 or later (GPL-2.0-or-later), as provided in
LICENSES/preferred/GPL-2.0.

The OpenOCD documentation is provided under the terms of the GNU Free
Documentation License version 1.2 or later without Invariant Sections
(GFDL-1.2-no-invariants-or-later).

Few stand-alone applications coexist in the same code tree of OpenOCD
and are provided under the terms of the GNU General Public License
version 3 (GPL-3.0), as provided in LICENSES/stand-alone/GPL-3.0.

This documentation file provides a description of how each source file
should be annotated to make its license clear and unambiguous.
It doesn't replace the OpenOCD's license.

The license described in the COPYING file applies to the OpenOCD source
as a whole, though individual source files can have a different license
which is required to be compatible with the GPL-2.0:

    GPL-1.0-or-later  : GNU General Public License v1.0 or later
    GPL-2.0-or-later  : GNU General Public License v2.0 or later
    LGPL-2.0          : GNU Library General Public License v2 only
    LGPL-2.0-or-later : GNU Library General Public License v2 or later
    LGPL-2.1          : GNU Lesser General Public License v2.1 only
    LGPL-2.1-or-later : GNU Lesser General Public License v2.1 or later

Aside from that, individual files can be provided under a dual license,
e.g. one of the compatible GPL variants and alternatively under a
permissive license like BSD, MIT etc.

The common way of expressing the license of a source file is to add the
matching boilerplate text into the top comment of the file. Due to
formatting, typos etc. these "boilerplates" are hard to validate for
tools which are used in the context of license compliance.

An alternative to boilerplate text is the use of Software Package Data
Exchange (SPDX) license identifiers in each source file. SPDX license
identifiers are machine parsable and precise shorthands for the license
under which the content of the file is contributed. SPDX license
identifiers are managed by the SPDX Workgroup at the Linux Foundation and
have been agreed on by partners throughout the industry, tool vendors, and
legal teams. For further information see https://spdx.org/

OpenOCD requires the precise SPDX identifier in all source files.
The valid identifiers used in OpenOCD are explained in the section
`License identifiers` and have been retrieved from the official SPDX
license list at https://spdx.org/licenses/ along with the license texts.

License identifier syntax
-------------------------

1. Placement:

   The SPDX license identifier in OpenOCD files shall be added at the
   first possible line in a file which can contain a comment. For the
   majority of files this is the first line, except for scripts which
   require the '#!PATH_TO_INTERPRETER' in the first line. For those
   scripts the SPDX identifier goes into the second line.

2. Style:

   The SPDX license identifier is added in form of a comment. The comment
   style depends on the file type::

      C source:  // SPDX-License-Identifier: <SPDX License Expression>
      C header:  /* SPDX-License-Identifier: <SPDX License Expression> */
      ASM:       /* SPDX-License-Identifier: <SPDX License Expression> */
      makefiles: # SPDX-License-Identifier: <SPDX License Expression>
      scripts:   # SPDX-License-Identifier: <SPDX License Expression>
      texinfo:   @c SPDX-License-Identifier: <SPDX License Expression>
      text:      # SPDX-License-Identifier: <SPDX License Expression>

   If a specific tool cannot handle the standard comment style, then the
   appropriate comment mechanism which the tool accepts shall be used. This
   is the reason for having the "/\* \*/" style comment in C header
   files. There was build breakage observed with generated .lds files where
   'ld' failed to parse the C++ comment. This has been fixed by now, but
   there are still older assembler tools which cannot handle C++ style
   comments.

3. Syntax:

   A <SPDX License Expression> is either an SPDX short form license
   identifier found on the SPDX License List, or the combination of two
   SPDX short form license identifiers separated by "WITH" when a license
   exception applies. When multiple licenses apply, an expression consists
   of keywords "AND", "OR" separating sub-expressions and surrounded by
   "(", ")" .

   License identifiers for licenses like [L]GPL with the 'or later' option
   are constructed by using a "-or-later":

      // SPDX-License-Identifier: GPL-2.0-or-later
      // SPDX-License-Identifier: LGPL-2.1-or-later

   WITH should be used when there is a modifier to a license needed.
   Exceptions can only be used with particular License identifiers. The
   valid License identifiers are listed in the tags of the exception text
   file.

   OR should be used if the file is dual licensed and only one license is
   to be selected. For example, some source files are available under dual
   licenses:

      // SPDX-License-Identifier: GPL-2.0-or-later OR BSD-1-Clause
      // SPDX-License-Identifier: GPL-2.0-or-later OR BSD-2-Clause
      // SPDX-License-Identifier: GPL-2.0-or-later OR BSD-3-Clause

   AND should be used if the file has multiple licenses whose terms all
   apply to use the file. For example, if code is inherited from another
   project and permission has been given to put it in OpenOCD, but the
   original license terms need to remain in effect::

      // SPDX-License-Identifier: GPL-2.0-or-later AND MIT

License identifiers
-------------------

The licenses currently used, as well as the licenses for code added to
OpenOCD, can be broken down into:

1. `Preferred licenses`:

   Whenever possible these licenses should be used as they are known to be
   fully compatible and widely used. These licenses are available from the
   directory:

      LICENSES/preferred/

   in the OpenOCD source tree.

   The files in this directory contain the full license text and
   `Metatags`. The file names are identical to the SPDX license
   identifier which shall be used for the license in source files.

   Examples:

      LICENSES/preferred/GPL-2.0

   Contains the GPL version 2 license text and the required metatags.

   `Metatags`:

   The following meta tags must be available in a license file:

   - Valid-License-Identifier:

     One or more lines which declare which License Identifiers are valid
     inside the project to reference this particular license text. Usually
     this is a single valid identifier, but e.g. for licenses with the 'or
     later' options two identifiers are valid.

   - SPDX-URL:

     The URL of the SPDX page which contains additional information related
     to the license.

   - Usage-Guidance:

     Freeform text for usage advice. The text must include correct examples
     for the SPDX license identifiers as they should be put into source
     files according to the `License identifier syntax` guidelines.

   - License-Text:

     All text after this tag is treated as the original license text

   File format examples::

      Valid-License-Identifier: GPL-2.0-only
      Valid-License-Identifier: GPL-2.0-or-later
      SPDX-URL: https://spdx.org/licenses/GPL-2.0.html
      Usage-Guide:
        To use this license in source code, put one of the following SPDX
        tag/value pairs into a comment according to the placement
        guidelines in the licensing rules documentation.
        For 'GNU General Public License (GPL) version 2 only' use:
          SPDX-License-Identifier: GPL-2.0-only
        For 'GNU General Public License (GPL) version 2 or any later version' use:
          SPDX-License-Identifier: GPL-2.0-or-later
      License-Text:
        Full license text

2. Exceptions:

   Some licenses can be amended with exceptions which grant certain rights
   which the original license does not.  These exceptions are available
   from the directory::

      LICENSES/exceptions/

   in the OpenOCD source tree.  The files in this directory contain the full
   exception text and the required `Exception Metatags`_.

   Examples::

      LICENSES/exceptions/eCos-exception-2.0

   Exception Metatags:

   The following meta tags must be available in an exception file:

   - SPDX-Exception-Identifier:

     One exception identifier which can be used with SPDX license
     identifiers.

   - SPDX-URL:

     The URL of the SPDX page which contains additional information related
     to the exception.

   - SPDX-Licenses:

     A comma separated list of SPDX license identifiers for which the
     exception can be used.

   - Usage-Guidance:

     Freeform text for usage advice. The text must be followed by correct
     examples for the SPDX license identifiers as they should be put into
     source files according to the `License identifier syntax`_ guidelines.

   - Exception-Text:

     All text after this tag is treated as the original exception text

   File format examples::

      SPDX-Exception-Identifier: eCos-exception-2.0
      SPDX-URL: https://spdx.org/licenses/eCos-exception-2.0.html
      SPDX-Licenses: GPL-2.0-only, GPL-2.0-or-later
      Usage-Guide:
        This exception is used together with one of the above SPDX-Licenses.
        To use this exception add it with the keyword WITH to one of the
        identifiers in the SPDX-Licenses tag:
          SPDX-License-Identifier: <SPDX-License> WITH eCos-exception-2.0
      License-Text:
        Full license text

3. Stand-alone licenses:

   These licenses should only be used for stand-alone applications that are
   distributed with OpenOCD but are not included in the OpenOCD binary.
   These licenses are available from the directory:

     LICENSES/stand-alone/

   in the OpenOCD source tree.

   Examples:

     SPDX-License-Identifier: GPL-3.0

The format and requirements of the license files in the other sub-directories
of directory

   LICENSES

have to follow the same format and requirements of the `Preferred licenses`.

All SPDX license identifiers and exceptions must have a corresponding file
in the LICENSES subdirectories. This is required to allow tool
verification (e.g. checkpatch.pl) and to have the licenses ready to read
and extract right from the source, which is recommended by various FOSS
organizations, e.g. the `FSFE REUSE initiative <https://reuse.software/>`.