/** @remote_bitbangpage OpenOCD Developer's Guide

The remote_bitbang JTAG+SWD driver is used to drive JTAG and/or SWD from a
remote process. The remote_bitbang driver communicates via TCP or UNIX
sockets with some remote process using an ASCII encoding of the bitbang
interface. The remote process presumably then drives the JTAG/SWD however
it pleases. The remote process should act as a server, listening for
connections from the openocd remote_bitbang driver.

The remote bitbang driver is useful for debugging software running on
processors which are being simulated.

There also is an implementation of the server-side protocol for the
Glasgow Debug Tool (https://github.com/glasgowEmbedded/Glasgow) through
the jtag-openocd applet.

The bitbang interface consists of the following functions.

blink on
	Blink a light somewhere. The argument on is either 1 or 0.

read
	Sample the value of tdo.

write tck tms tdi
	Set the value of tck, tms, and tdi.

reset trst srst
	Set the value of trst, srst.

swdio_drive
	Set the output enable of the bidirectional swdio (tms) pin

swdio_read
	Sample the value of swdio (tms).

swd_write
	Set the value of swclk (tck) and swdio (tms).

(optional) sleep
	Instructs the remote host to sleep/idle for some period of time before
		executing the next request

An additional function, quit, is added to the remote_bitbang interface to
indicate there will be no more requests and the connection with the remote
driver should be closed.

The eight mandatory functions are encoded in ASCII by assigning a single
character to each possible request. The assignments are:

	B - Blink on
	b - Blink off
	R - Read request
	Q - Quit request
	0 - Write 0 0 0
	1 - Write 0 0 1
	2 - Write 0 1 0
	3 - Write 0 1 1
	4 - Write 1 0 0
	5 - Write 1 0 1
	6 - Write 1 1 0
	7 - Write 1 1 1
	r - Reset 0 0
	s - Reset 0 1
	t - Reset 1 0
	u - Reset 1 1
	O - SWDIO drive 1
	o - SWDIO drive 0
	c - SWDIO read request
	d - SWD write 0 0
	e - SWD write 0 1
	f - SWD write 1 0
	g - SWD write 1 1

The read responses are encoded in ASCII as either digit 0 or 1.

If the use_remote_sleep option is set to 'yes', two additional requests may
be sent:

	Z - Sleep for 1 millisecond
	z - Sleep for 1 microsecond

NOTE: Previously these were specified as 'D' and 'd', which conflicts with the
"SWD write 0 0" command defined above. Adapters that implement Dd for remote
sleep must be updated to work with Zz.


 */