git-backfill(1)
===============

NAME
----
git-backfill - Download missing objects in a partial clone


SYNOPSIS
--------
[verse]
(EXPERIMENTAL) 'git backfill' [--batch-size=<n>] [--[no-]sparse]

DESCRIPTION
-----------

Blobless partial clones are created using `git clone --filter=blob:none`
and then configure the local repository such that the Git client avoids
downloading blob objects unless they are required for a local operation.
This initially means that the clone and later fetches download reachable
commits and trees but no blobs. Later operations that change the `HEAD`
pointer, such as `git checkout` or `git merge`, may need to download
missing blobs in order to complete their operation.

In the worst cases, commands that compute blob diffs, such as `git blame`,
become very slow as they download the missing blobs in single-blob
requests to satisfy the missing object as the Git command needs it. This
leads to multiple download requests and no ability for the Git server to
provide delta compression across those objects.

The `git backfill` command provides a way for the user to request that
Git downloads the missing blobs (with optional filters) such that the
missing blobs representing historical versions of files can be downloaded
in batches. The `backfill` command attempts to optimize the request by
grouping blobs that appear at the same path, hopefully leading to good
delta compression in the packfile sent by the server.

By default, `git backfill` downloads all blobs reachable from the `HEAD`
commit. This set can be restricted or expanded using various options.

OPTIONS
-------

--batch-size=<n>::
	Specify a minimum size for a batch of missing objects to request
	from the server. This size may be exceeded by the last set of
	blobs seen at a given path. Default batch size is 16,000.

--[no-]sparse::
	Only download objects if they appear at a path that matches the
	current sparse-checkout. If the sparse-checkout feature is enabled,
	then `--sparse` is assumed and can be disabled with `--no-sparse`.

SEE ALSO
--------
linkgit:git-clone[1].

GIT
---
Part of the linkgit:git[1] suite