target_sdk_dir=""
post_install_cleanup=1
confirm=0

usage () {
  cat << EOF
  Usage : $TOOLCHAIN_NAME < -- options >


Options:
  -h
        Display this help and exit.

  -d <dir>
        Specify the absolute path of the SDK installation directory.

  -y
        Automatic yes to prompts; assume "yes" as answer to all prompts.

EOF
}

verify_os () {
case "$(uname -s)" in

   Darwin)
     echo 'OS X is not supported!'
     exit 1
     ;;

   # Linux, the only supported OS

   Linux)
     #echo 'Linux'
     ;;

   # Other OS ...
   # see https://en.wikipedia.org/wiki/Uname#Examples
   # Don't allow to install on any of them, this includes cygwin, Windows,
   # Solaris etc.

   *)
     echo 'Unsupported OS'
     exit 1
     ;;
esac
}

while [ "$1" != "" ]; do
	case $1 in
	    -h )
			usage
			exit 0
			;;
		-d )
			shift
			target_sdk_dir=$1
			;;
		-nocleanup )
			post_install_cleanup=0;
			;;
		-y )
			confirm="y";
			;;
		* )
			echo "Error: Invalid argument \"$1\""
			usage
			exit 1
			;;
	esac
	shift
done

spinner()
{
	local pid=$1
	local delay=0.175
	local spinstr='|/-\'
	local infotext=$2
	while kill -0 $pid 2>/dev/null ; do
		local temp=${spinstr#?}
		printf " [%c] %s" "$spinstr" "$infotext"
		local spinstr=$temp${spinstr%"$temp"}
		sleep $delay
		printf "\b\b\b\b\b\b"
		for i in $(seq 1 ${#infotext}); do
			printf "\b"
		done
	done
	printf " [*] %s" "$infotext"
	printf " \b\b\b\b"
}

do_cleanup()
{
	cd $target_sdk_dir
	if [ $post_install_cleanup = "1" ]; then
		#rm site-config*
		rm environment-setup*
	fi
	install -d -m 0755 $VERSION_DIR
	mv version-* $VERSION_DIR
	echo "$SDK_VERSION" > sdk_version
	chmod 0644 sdk_version
}

# Read the input "y"
read_confirm () {
    echo "The directory $target_sdk_dir/sysroots will be removed! "
  if [ "$confirm" != "y" ]; then
      echo "Do you want to continue (y/n)? "
      while read confirm; do
          [ "$confirm" = "Y" -o "$confirm" = "y" -o "$confirm" = "n" \
            -o "$confirm" = "N" ] && break
          echo "Invalid input \"$confirm\", please input 'y' or 'n': "
      done
  else
      echo
  fi
}

verify_os

which python3 2>&1 > /dev/null
if [ $? -ne 0 ]; then
	echo "ERROR: required python3 binary not in PATH" 1>&2
	exit 1
fi

which xz 2>&1 > /dev/null
if [ $? -ne 0 ]; then
	echo "ERROR: required xz binary not in PATH" 1>&2
	exit 1
fi

if [ "$target_sdk_dir" = "" ]; then
	read -e -p "Enter target directory for SDK (default: $DEFAULT_INSTALL_DIR): " target_sdk_dir
	[ "$target_sdk_dir" = "" ] && target_sdk_dir=$DEFAULT_INSTALL_DIR
fi

eval target_sdk_dir=$target_sdk_dir

if [[ $target_sdk_dir != /* ]]; then
	echo "The target directory path ($target_sdk_dir) must be an absolute path. Abort!"
	exit 1;
fi

eval target_sdk_dir=$(echo "$target_sdk_dir"|sed 's/ /\\ /g')
if [ -d "$target_sdk_dir" ]; then
	target_sdk_dir=$(cd "$target_sdk_dir"; pwd)
else
	target_sdk_dir=$(readlink -m "$target_sdk_dir")
fi

if [ -n "$(echo $target_sdk_dir|grep ' ')" ]; then
	echo "The target directory path ($target_sdk_dir) contains spaces. Abort!"
	exit 1
fi

echo "Installing SDK to $target_sdk_dir"

if [ -d $target_sdk_dir ]; then
	# If the directory exists, test for write permission
	if [ ! -w $target_sdk_dir ] ; then
		echo "No permission, please run as 'sudo'"
		exit 1
	else
		# wipe the directory first
		if [ -d $target_sdk_dir/sysroots ]; then
		read_confirm
	    if [ "$confirm" = "y" -o "$confirm" = "Y" ]; then
		        rm -rf $target_sdk_dir/sysroots/
			rm -rf $target_sdk_dir/info-zephyr-sdk*/
			rm -fr $target_sdk_dir/sdk_version
		else
		    # Abort the installation
		    echo "SDK installation aborted!"
		    exit 1
		    fi
		fi
	fi
else
	echo "Creating directory $target_sdk_dir"
	# Try to create the directory (this will not succeed if user doesn't have rights)
	if install -d -m 0751 $target_sdk_dir >/dev/null 2>&1  ; then
		echo "Success"
	else
		echo "No permission, please run as 'sudo'"
		exit 1
	fi
fi

if (( EUID != 0 )); then
	umask 0002
#else
#	umask 0022
fi