@echo off

REM # Automated setup script for Zephyr SDK distribution bundle archive
REM # for Windows host operating system

pushd %~dp0
setlocal ENABLEDELAYEDEXPANSION
set EXITCODE=0

goto entry

REM # Check if command is available
:check_command
where %1 > nul 2>&1
if [%ERRORLEVEL%] neq [0] (
  echo Zephyr SDK setup requires '%1' to be installed and available in the PATH.
  echo Please install '%1' and run this script again.

  set EXITCODE=%2
  exit /b 1
)
exit /b 0

:entry

REM # Initialise toolchain list
set TOOLCHAINS=
for /f %%t in (sdk_toolchains) do (
  set TOOLCHAINS=!TOOLCHAINS! %%t
)

REM Initialise list of toolchains to install
set INST_TOOLCHAINS=

REM # Read bundle version from file
set /p VERSION=<sdk_version

REM # Resolve release download base URI
set DL_REL_BASE=https://github.com/zephyrproject-rtos/sdk-ng/releases/download/v%VERSION%
set DL_TOOLCHAIN_FILENAME=toolchain_windows-x86_64_%%t.7z

REM # Print banner
echo Zephyr SDK %VERSION% Setup
echo.

REM # Enable interactive mode if no argument is specified
if [%1] equ [] (
  set INTERACTIVE=y
)

REM # Check dependencies

call :check_command cmake 90
if [%ERRORLEVEL%] neq [0] goto end
call :check_command wget 91
if [%ERRORLEVEL%] neq [0] goto end
call :check_command 7z 92
if [%ERRORLEVEL%] neq [0] goto end

REM # Enter interactive mode if enabled
if [%INTERACTIVE%] neq [] (
  goto interactive
)

REM # Parse arguments if specified
:parsearg
if /i [%1] equ [/t] (
  if [%2] equ [all] (
    set INST_TOOLCHAINS=%TOOLCHAINS%
  ) else (
    set IS_VALID=
    for %%t in (%TOOLCHAINS%) do if [%%t] equ [%2] set IS_VALID=y
    if [!IS_VALID!] equ [y] (
      set INST_TOOLCHAINS=!INST_TOOLCHAINS! %2
    ) else (
      echo ERROR: Unknown toolchain '%2'
      set EXITCODE=2
      goto end
    )
  )
  shift
) else if /i [%1] equ [/h] (
  set DO_HOSTTOOLS=y
) else if /i [%1] equ [/c] (
  set DO_CMAKE_PKG=y
) else (
  goto usage
)

shift
if [%1] neq [] (
  goto parsearg
)

goto process

:interactive
REM # Print interactive mode informational message
echo ** NOTE **
echo You only need to run this script once after extracting the Zephyr SDK
echo distribution bundle archive.
echo.

REM # Check installation type
for %%t in (%TOOLCHAINS%) do (
  if not exist %%t\ (
    set IS_PARTIAL_SDK=y
  )
)

REM # Ask user for set-up choices
if [%IS_PARTIAL_SDK%] neq [] (
  choice /c:yn /m:"Install toolchains for all targets"
  if [!ERRORLEVEL!] equ [1] (
    set INST_TOOLCHAINS=%TOOLCHAINS%
  ) else (
    for %%t in (%TOOLCHAINS%) do (
      if not exist %%t\ (
        choice /c:yn /m:"Install '%%t' toolchain"
        if [!ERRORLEVEL!] equ [1] (
          set INST_TOOLCHAINS=!INST_TOOLCHAINS! %%t
        )
      )
    )
  )
)

choice /c:yn /m:"Install host tools"
if [%ERRORLEVEL%] equ [1] set DO_HOSTTOOLS=y

choice /c:yn /m:"Register Zephyr SDK CMake package"
if [%ERRORLEVEL%] equ [1] set DO_CMAKE_PKG=y

echo.

:process
REM # Install toolchains
for %%t in (%INST_TOOLCHAINS%) do (
  set TOOLCHAIN_FILENAME=%DL_TOOLCHAIN_FILENAME%
  set TOOLCHAIN_URI=%DL_REL_BASE%/!TOOLCHAIN_FILENAME!

  if not exist %%t\ (
    echo Installing '%%t' toolchain ...

    REM # Download toolchain archive
    wget -q --show-progress -N -O !TOOLCHAIN_FILENAME! !TOOLCHAIN_URI!
    if [!ERRORLEVEL!] neq [0] (
      del /q !TOOLCHAIN_FILENAME!
      echo ERROR: Toolchain download failed
      set EXITCODE=20
      goto end
    )

    REM # Extract archive
    7z x -o. !TOOLCHAIN_FILENAME!
    if [!ERRORLEVEL!] neq [0] (
      echo ERROR: Toolchain archive extraction failed
      set EXITCODE=21
      goto end
    )

    REM # Remove archive
    del /q !TOOLCHAIN_FILENAME!
  )
)

REM # Install host tools
if [%DO_HOSTTOOLS%] neq [] (
  echo Installing host tools ...
  echo SKIPPED: Windows host tools are not available yet.
  echo.
)

REM # Register Zephyr SDK CMake package
if [%DO_CMAKE_PKG%] neq [] (
  echo Registering Zephyr SDK CMake package ...
  cmake -P cmake\zephyr_sdk_export.cmake
  if [!ERRORLEVEL!] neq [0] (
    set EXITCODE=40
    goto end
  )
  echo.
)

echo All done.
goto end

REM # Print scripting mode usage
:usage
echo %~n0 [/t ^<toolchain^>] [/h] [/c]
echo.
echo   /t ^<toolchain^>   Install specified toolchain
echo      all           Install all toolchains
echo   /h               Install host tools
echo   /c               Register Zephyr SDK CMake package
echo.
echo Supported Toolchains:
echo.
for %%t in (%TOOLCHAINS%) do (
  echo %%t
)
echo.
echo When no arguments are specified, the setup script runs in the interactive
echo mode asking for user inputs.

set EXITCODE=1

:end
if [%INTERACTIVE%] neq [] (
  echo.
  echo Press any key to exit ...
  pause > nul
)

popd

exit /b %EXITCODE%